AC to DC Conversion FAQs

FAQ

Can fuses with an AC voltage rating be used in a DC applications?

Fuses must be rated for the voltage AC or DC in which they will be used. Generally, fuses have a DC voltage rating that is half of the maximum AC voltage rating. (Example: LLSRK_ID - 600 VAC, 300VDC) Consult the factory for specific DC voltage ratings.