ࡱ> %` ;bjbjNN 4,,2[    * 666JVpVpVp8p\pJj,rrrrrss t$h^6tsstt66rr4$[y[y[ytv6r6r[yt[y[yr)T66rr \!Vpeu^}͆:0j\u,\\64 t".t[yFtZt t t twl t t tjttttJJN!*2L$$JJN!2LJJJ666666 ENGINEERING SPECIFICATION SYMCOM MODEL 777-LR-TS Electronic Overload Relay GENERAL REFERENCES UL 508 Industrial Control Equipment Underwriters Laboratories IEC 60947 Low Voltage Switchgear and Controlgear International Electrotechnical Commission CSA C22.2 No. 14 Industrial Control Equipment Canadian Standards Association ANSI/IEEE C62.41 American National Standards Institute/Institute of Electrical & Electronics Engineers MODBUS over Serial Line Specification and Implementation Guide V1.02 UL 1053 Ground-Fault Sensing and Relaying Equipment Underwriters Laboratories WARRANTY Manufacturer Warranty: The manufacturer shall guarantee the overload relay to be free from material and workmanship defects for a period of five years from the date of manufacture when installed and operated according to the manufacturers requirements. PRODUCTS MANUFACTURERS The equipment specified shall be the Model 777-LR-TS, manufactured by SymCom, Inc. DESCRIPTION Regulatory Requirements: The equipment shall be UL Listed as type NKCRIndustrial Control Equipment-Motor Controllers-Auxiliary Devices. The equipment shall be ULC Listed as type NKCR7Industrial Control Equipment-Motor Controllers-Auxiliary Devices Certified for Canada. The equipment shall be CE marked for use in the European Union and evaluated against IEC 60947 Low Voltage Switchgear and Controlgear. The equipment shall be CSA certified as class 3211-03Industrial Control Equipment-Motor Controllers-Auxiliary Devices. Performance/Design Criteria: 3-PHASE ELECTRONIC OVERLOAD RELAY Protective Relay Functions The equipment shall provide protection against the following conditions: voltage single phase/phase loss phase reversal low voltage high voltage voltage unbalance rapid cycling to prevent on-off cycling of the motor in rapid succession undercurrent overcurrent current unbalance current single phase/phase loss ground fault contact failure, to trip the motor, if the motor starter is damaged which causes a current single phase. hot/temperature sensing Communication Capabilities The equipment shall provide Modbus RTU communications capabilities when combined with the appropriate SymCom network communications modules. Visit www.symcom.com for the current list of communication modules. The equipment interface shall have the capability of connecting to the following systems: HMI (Human Machine Interface) SCADA (Supervisory Control and Data Acquisition) programs. DCS (Distributed Control System) PLC (Programmable Logic Controllers) The equipment shall support 9600 baud, Even parity, and 1 stop bit. The equipment shall provide set points that are readable and writable via the Modbus interface. The equipment shall provide the ability to energize and de-energize the motor via the Modbus interface. The equipment shall provide a 10-second Modbus network watchdog to trip the relay when Modbus communication is lost. Network Capabilities The equipment shall provide registers to read the following real-time values: L1-L2 line voltage L2-L3 line voltage L3-L1 line voltage Average line voltage Phase A current Phase B current Phase C current Average phase current Voltage unbalance Current unbalance Current multiplier Power factor Ground fault current Restart Delay 1 (RD1) Time Remaining Restart Delay 2 (RD2) Time Remaining Restart Delay 3 (RD3) Time Remaining Power in KW Trip status of the following: Manual reset status Network off command status Contact failure Undercurrent Overcurrent Ground fault Current unbalance Current single phase Temperature sensing Status of the following: Low voltage pending High voltage pending Voltage unbalance pending Undercurrent pending Reverse phase pending Current unbalance pending Voltage single phase pending Current single phase pending Over current pending Ground fault pending Relay status Last fault 1 Last fault 2 Last fault 3 Last fault 4 Unit ID Model code Motor run hours The equipment shall provide the following readable/writable setpoints: Low voltage trip point High voltage trip point Voltage unbalance trip point Current multiplier, used to scale the current reading properly when Current Transformers (CTs) or amp turns are used Overcurrent trip point Undercurrent trip point Current unbalance trip point Trip class setpoint Restart delay 1 setpoint Restart delay 2 setpoint Restart delay 3 setpoint Number of restarts after an undercurrent fault (#RU) setpoint Number of restarts after a fault (#RF) setpoint Undercurrent trip delay setpoint Ground fault trip point Modbus address setpoint Temperature sensing on/off Trip enable setpoint to enable the following: Ground Fault trip Voltage Unbalance trip Current Unbalance trip Undercurrent trip Command line to respond to the following commands: Network program enable Network program disable Clear run hours Clear fault history Enable network watchdog Disable network watchdog Start the motor Stop the motor Capabilities and Features Inputs The equipment shall require a 3-phase input voltage of 200-480VAC. The equipment shall accept full load current of 1-9 amps. The equipment shall require a 3-phase 50/60 Hz input voltage. The equipment shall provide connection to an external remote reset switch. Outputs The equipment shall include one Form C (SPDT) output relay. Contacts pilot duty rated 480VA@240VAC. Contacts general purpose rated 10A@240VAC. Functional Specifications The equipment shall include the following front panel setpoint ranges: an adjustable low voltage (LV) setpoint range of 170-524VAC an adjustable high voltage (HV) setpoint range of 172-528VAC an adjustable voltage unbalance (VUB) setpoint range of 2-15% or 999 (disabled) a temperature sensor (TS) setpoint of ON or oFF an adjustable multiplier (MULT) setpoint range of 1 or 2 an adjustable overcurrent (OC) setpoint range of (20-100A) MULT or 80-120% of CT Primary an adjustable undercurrent (UC) setpoint range of (0, 10-98A) MULT or 40-100% of CT Primary an adjustable current unbalance (CUB) setpoint range of 2-25% or 999 (disabled) an adjustable trip class (TC) setpoint range of 05,J05,10,J10,15,J15,20,J20,30,J30 an adjustable rapid-cycle timer 1 (RD1) of 0-500 seconds an adjustable motor cool-down timer (RD2) of 2-500 minutes an adjustable undercurrent restart delay timer (RD3) of 2-500 minutes, A (automatic) an adjustable number of restarts after undercurrent (#RU) setpoint range of 0-4, A (automatic) an adjustable device communication address (ADDR) setpoint range of A01-A99 an adjustable number of restarts after all other faults (#RF) setpoint range of 0, 1, oc1, 2, oc2, 3, oc3, 4, oc4, A, or ocA, where an oc prefix means that over current trips are included in the restart counts, otherwise over current is not included. an adjustable undercurrent trip delay (UCTD) setpoint range of 2-60 seconds an adjustable ground fault current (GF) setpoint range of (3-20A) MULT or 10-30% of CT Primary or oFF The equipment shall provide ground fault protection that meets UL1053 requirements. The equipment shall provide three independent adjustable restart delays, one for power-up and rapid-cycle protection, one for overcurrent, current unbalance and current single phasing (contact failure), and another one for undercurrent faults. The equipment shall provide an undercurrent trip delay. The equipment shall allow manual or automatic restart after a fault. The equipment shall have the ability to display the last fault that caused the relay to trip off. The equipment shall provide a jam feature that trips the relay if any current phase exceeds 400% of the OC setpoint, 1 minute after start up. The equipment shall provide a method to enable/disable the following trip conditions: Ground Fault Voltage Unbalance Current Unbalance Undercurrent Temperature Sensing The equipment shall provide a motor run hour meter. The equipment shall provide a front panel tamper guard, to prevent accidental setpoint changes. The equipment shall provide the ability to clear the last fault using the front panel. The equipment shall provide automatic restart timing after undercurrent when RD3 is set to A. Run time >1 hr the next restart delay will be 6 minutes Run time 30-59.99 minutes the next restart delay will be 15 minutes Run time 15-29.99 minutes the next restart delay will be 30 minutes Run time <15 minutes the next restart delay will be 60 minutes Timing Requirements The equipment shall provide a ground fault trip delay that follows an inverse time curve with a maximum trip time of 8 seconds and a minimum trip time of 2 seconds. The equipment shall provide a current unbalance trip delay that follows an inverse time curve with a maximum trip time of 30 seconds and a minimum trip time of 2 seconds. The equipment shall provide an overload trip time that follows an inverse time trip curve. Accuracy Requirements The equipment shall provide a timing accuracy on all timers of 5% 1 second. The equipment shall provide a current measurement accuracy of 3% for currents <100 amps direct for A, B, C phase currents. The equipment shall provide a ground fault current measurement accuracy of 15% for currents <100 amps direct. The equipment shall provide a voltage measurement accuracy of 1%. Human Interface Features The equipment shall provide an adjustment dial to set the following setpoints: Low Voltage (LV) High Voltage (HV) Voltage Unbalance (VUB) Temperature Sensing (TS) Multiplier (MULT) Overcurrent (OC) Undercurrent (UC) Current Unbalance (CUB) Trip Class (TC) Rapid-Cycle Timer (RD1) Motor Cool-Down Timer (RD2) Undercurrent Restart Delay Timer (RD3) Number Of Restarts After Undercurrent (#RU) Device Communication Address (ADDR) Number Of Restarts After Other Faults (#RF) Undercurrent Trip Delay (UCTD) Ground Fault (GF) The equipment shall provide and adjustment dial to view the following runtime information: L1-L2 line voltage L2-L3 line voltage L3-L1 line voltage Average line voltage A phase current B phase current C phase current Average phase current The equipment shall provide a 3-digit 7-segment display for viewing operating parameters of the device. The equipment shall provide a push button switch for the following functions: Programming the device Viewing the last fault Resetting the device after a fault Resetting the device during a restart delay Electromagnetic Compatibility The equipment shall be immune to electrostatic discharge per IEC 61000-4-2, Level 3, 6kV contact discharge and 8kV air discharge. The equipment shall be immune to electrical fast transient bursts exceeding IEC 61000-4-4, Level 3. Specified limits shall be 3.5kV input power. The equipment shall be immune to electrical surges per IEC 61000-4-5, Level 3. Specified limits shall be 2kV line-to-line; Level 4, 4kV line-to-ground. The equipment shall be immune to surge and ring wave per ANSI/IEEE C62.41. Specified limits shall be 6kV line-to-line. The equipment shall be immune to radiated radio frequency emissions per IEC 61000-4-3, Level 3. Specified limits shall be 10V/m. The equipment shall be immune to conducted radio frequency emissions per IEC 61000-4-6, Level 3. Specified limits shall be 10V. Vibration/Shock Requirements The equipment shall withstand vibrations per IEC 68-2-6. Specified limits shall be 10-55Hz, 1mm peak-to-peak, 2 hours, 3 axis. The equipment shall withstand shocks per IEC 68-2-27. Specified limits shall be 30g, 3 axis, 11ms duration, half-sine pulse. Dielectric Isolation: Equipment withstands an alternating current potential of 1000V plus twice the rated voltage of the equipment for 1 minute without breakdown between uninsulated live parts and the enclosure with the contacts open and closed; between terminals of opposite polarity with the contacts closed; and between uninsulated live parts of different circuits. Enclosure Class of Protection: The equipment shall provide IEC IP20 (finger safe) protection. Short Circuit Requirements The equipment shall provide a short circuit rating of 100kA. Environmental Requirements The equipment shall operate continuously without de-rating in ambient temperatures of -20 to 70C (-4 to 158F). The equipment shall operate continuously without de-rating in relative humidity of up to 95% non-condensing per IEC 68-2-3. The equipment shall operate properly after storage in ambient temperatures of -40 to 80C (-40 to 176F). Dimensions: The equipment dimensions shall not exceed 3.0 in height X 3.6 in width X 5.1 in depth. Mounting: The equipment shall be mountable on standard 35 mm DIN rail. The equipment shall be surface mountable on a backplane. Conformal coating: The equipment shall contain harsh environment conformal coating to help extend product life and to protect from hostile environments including moisture, temperature variations, salt spray, organic attack (fungus), and aggressive chemicals and vapors. En SEQ CHAPTER \h \r 1d of Section  Temperature sensing trip feature supported by Subtrol -equipped pumps. Subtrol is a registered trademark of Franklin Electric Co., Inc.        4- ES-777-LR-TS 06/2010 '+.01;KL`f * K L J K L M 򿭜|||jX|#hrDhQ#5CJOJQJ^JaJ#hhQ#5CJOJQJ^JaJ#h]hQ#5CJOJQJ^JaJhQ#CJOJQJ^JaJ h^_hQ#CJOJQJ^JaJ#h^_hQ#5CJOJQJ^JaJhQ#CJOJQJ^Jh+n5CJOJQJ^Jh 5CJOJQJ^Jh 5CJOJQJ^JhQ#5CJOJQJ^JKLTJ<$ & F \`0@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#;$ \0b@ P !$`'0*-/2p5@8;=@CPF Idh1$a$gdQ#=$ \0b@ P !$`'0*-/2p5@8;=@CPF Idh1$@&a$gdQ#:9;;TU`L K HHHHHH:$ & F Y`0@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ & F \`0@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#?$ \`0@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#K L M V |A:$ & F Y`08@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#?$ \`08@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#B$ b `0*8@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#M V o U W X Y r [ \ ] t v w k l m ⠒Ѯn``nnnh,CJOJQJ^JaJ#hxhQ#5CJOJQJ^JaJ#hChQ#5CJOJQJ^JaJh CJOJQJ^JaJh CJOJQJ^JaJ#h^_hQ#5CJOJQJ^JaJ h@zhQ#CJOJQJ^JaJ h^_hQ#CJOJQJ^JaJhQ#CJOJQJ^JaJhQ#5CJOJQJ^JaJ"V W X Y N8$ \`08@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#:$ & F Y`08@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ \`08@ P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#Y b c q H:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#?$ \`08@ P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#<$ & F \`08@ P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#q r M:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#8$ Y`0P !$`'0*-/2p5@8;=@CPF I1$@&a$gdQ#>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ# \ Q7$ & F S`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#\ ] l m NN<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#;$ S`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ# %&N7$ Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#?$ Y`0P !$`'0*-/2p5@8;=@CPF I01$^`0a$gdQ#  $%&gh%ǵvhvhvZvhL8hv'jhC0JCJOJQJU^JaJhu DCJOJQJ^JaJhQ6CJOJQJ^JaJhCCJOJQJ^JaJhQ#CJOJQJ^JaJ hhQ#CJOJQJ^JaJ h1mhQ#CJOJQJ^JaJh+n5CJOJQJ^JaJ#hhQ#5CJOJQJ^JaJ&hhQ#5;CJOJQJ^JaJ hQ#5;CJOJQJ^JaJ&h'hQ#5;CJOJQJ^JaJ&ABN:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#.;GYy 7$ Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ# $%P9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#%)69OPQRVY]opT_"+ӴӦӦӘӊ|nhCCJOJQJ^JaJhQ6CJOJQJ^JaJh 1CJOJQJ^JaJh,CJOJQJ^JaJh):CJOJQJ^JaJh^CJOJQJ^JaJ hyhQ#CJOJQJ^JaJhQ#CJOJQJ^JaJh6CJOJQJ^JaJ hzh6CJOJQJ^JaJ&QpPPP9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdQ#7P9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gd678yzLLL<$ V`0P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#zP9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#,<L\r:Fd9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#dx1F`u9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#noQRmt/z{䛍qqcqqRqRR h^_h 1CJOJQJ^JaJhCJOJQJ^JaJh 1CJOJQJ^JaJhlGCJOJQJ^JaJhYLCJOJQJ^JaJh7tCJOJQJ^JaJ hyhQ#CJOJQJ^JaJh^CJOJQJ^JaJhCCJOJQJ^JaJhQ6CJOJQJ^JaJhQ#CJOJQJ^JaJhLCJOJQJ^JaJ #0=JR]m9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ# mnvPPPPPPP9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ# !_);Ri{9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#2BQRlW9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#5$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ# lmt/zUUUU7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd 1:$ Y`0*P !$`'0*-/2p5@8;=@CPF Id1$a$gdQ#z{U7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t:$ Y`0*P !$`'0*-/2p5@8;=@CPF Id1$a$gda .@lmopPQ  V W ####~########ŷũq```` hyhQ#CJOJQJ^JaJheb,CJOJQJ^JaJhYLCJOJQJ^JaJh3CJOJQJ^JaJh*`CJOJQJ^JaJhQ#CJOJQJ^JaJh 1CJOJQJ^JaJh7tCJOJQJ^JaJ h^_h 1CJOJQJ^JaJh^CJOJQJ^JaJh<CJOJQJ^JaJ%.u@pbWWWWWWWW7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gdQ#  > y -!y!t""(#)#;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t )#}#~#r$s$$$$$T%U%%9&;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t #-$.$G$U$q$$$$$$%%R%o&p&w&&&&''((***E,F,,ַ֩֍qcR h^_hQ#CJOJQJ^JaJh<CJOJQJ^JaJhCJOJQJ^JaJhCJOJQJ^JaJhrCJOJQJ^JaJhu DCJOJQJ^JaJhCJOJQJ^JaJh^CJOJQJ^JaJ hyhQ#CJOJQJ^JaJhQ#CJOJQJ^JaJhQ6CJOJQJ^JaJht;CJOJQJ^JaJ9&F&X&j&w&&&&Q7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gd7t&&"'#'z'{''(U((TTT7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd17$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd7t;$ S`0*FP !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdQ# ((((V9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ68$ S`0*FP !$`'0*-/2p5@8;=@CPF I1$^a$gdQ67$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd1(())?*@**NN<$ V`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gd9$ & F V`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gd;$ S`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gd****+t;9$ & F V`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gdQ#$ `0d1$^a$gd<7$ & F S`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ V`0*FP !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#++++++4,5,O9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#9$ & F V`0*FP !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0*FP !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#5,N,O,,P9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#,,,,,--'-?-O-g-----&.E.W.:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#,,- ---T-U-q-r-----+.,.f/m/n/w/|0}000o1p1111133F3G3334T666 77:7_7`7777777 h^_hQ#CJOJQJ^JaJh7tCJOJQJ^JaJh<CJOJQJ^JaJhBCJOJQJ^JaJh 1CJOJQJ^JaJh,CJOJQJ^JaJh^CJOJQJ^JaJhQ#CJOJQJ^JaJhCJOJQJ^JaJ2W.X.....//!/MMMMMM:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#!/1/G/H//M9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#>$ Y`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#///0-0P0|0NNNN:$ & F Y`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#|0}000Q<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#8$ S`0*FP !$`'0*-/2p5@8;=@CPF I`1$^`a$gd01111K2L222F3G339 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdQ#6 & F V`0*P !$`'0*-/2p5@8;=@CPF I1$gdQ# 3333X9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdQ#6 & F V`0*P !$`'0*-/2p5@8;=@CPF I1$gdQ#6 V`0*P !$`'0*-/2p5@8;=@CPF I1$^gdQ#3e4f444P?$ Y`0*P !$`'0*-/2p5@8;=@CPF I1$^`a$gdQ#9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdQ#6 & F V`0*P !$`'0*-/2p5@8;=@CPF I1$gdQ#4U6V6666R9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#6677N< Y`0*P !$`'0*-/2p5@8;=@CPF I1$^`gdQ#7$ & F S`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#7+7,77S6 & F V`0*P !$`'0*-/2p5@8;=@CPF I1$gdQ#<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#7777777788+898Z8k8m8s8t8w8{888888888888;9r9s9t9u9999::´¢ve hJh7tCJOJQJ^JaJ h9hQ#CJOJQJ^JaJ h9hQ#CJOJQJ^JaJhQ#CJOJQJ#h hQ#5CJOJQJ^JaJh 1CJOJQJ^JaJ h15hQ#CJOJQJ^JaJh6CJOJQJ^JaJhQ#CJOJQJ^JaJ h^_hQ#CJOJQJ^JaJ'778888U9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#6 & F V`0*P !$`'0*-/2p5@8;=@CPF I1$gdQ#9 V`0*P !$`'0*-/2p5@8;=@CPF Id1$^gdQ#88888O<$ V`0P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ V`0P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#9$ & F V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#8:9;9t9u9L<$ V`0*P !$`'0*-/2p5@8;=@CPF I`d1$^`a$gdQ#<$ V`0*P !$`'0*-/2p5@8;=@CPF Id1$^a$gdQ#9$ & F V`0*P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#u999:V6 & F V`0*P !$`'0*-/2p5@8;=@CPF I1$gd7t9$ V`0*P !$`'0*-/2p5@8;=@CPF I1$^a$gdQ#9$ & F V`0*P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#::::::::::::::::::::::7;8;9;:;<;=;?;ʳhVhVRJRJRjh\.vUh\.v#hUeB*CJOJQJ^JaJph# ,hChUeB*CJH*OJQJ^JaJph# )hChUeB*CJOJQJ^JaJph# hUeCJOJQJ^JaJ hChUeCJOJQJ^JaJ-jhChUe0JCJOJQJU^JaJh}X+ h`chQ#hQ#CJOJQJ^JaJhQ#jhQ#U hChQ#CJOJQJ^JaJ:::8;9;;;<;>;?;A;B;D;E;F;/ V`0P !$`'0*-/2p5@8;=@CPF I1$;$ \0b@ P !$`'0*-/2p5@8;=@CPF Id1$a$gdQ# ?;@;B;C;E;G;H;K;L;O;P;T;x;z;{;|;};;;;;;Ͻh}X+ h}hUe,jh}hUe5CJOJQJU^JaJ#h}hUe5CJOJQJ^JaJhUeOJQJj hUeUjhUeUjhUeUhUeh\.vjh\.vUF;G;R;S;T;x;ff05$ V`0P !$`'0*-/2p5@8;=@CPF Id1$a$/ V`0P !$`'0*-/2p5@8;=@CPF I1$5$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$gdQ#2 V`0P !$`'0*-/2p5@8;=@CPF Id1$x;|;};;;;;5$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$gd 12$ V`0P !$`'0*-/2p5@8;=@CPF I1$a$2:pQ#BP/ =!"#$% Dd0*<DOR  S .ACE_logob*tzNm*D~n*tzNm*PNG  IHDRPLTE79de%&e2}bKGDHgIFg :Hf cmPPJCmp0712OmIDATxrֵդ)JES)J,8YO8Ydpw9nӦM <^֩33yyNx좝t{|Ex9?hNM]5s㫚ii?ί9Z岠ϔoEX9}{! rv.}|)Gc.vGY{f`.l \4\l ͥ@k2|U@2 Rchkޫ22>(+??$Vo7A(+ ŕz ڀVnuAȸ[9̙ X]yA 6C˺xsfp恦pN ™9#hg`j$$OVЍ02ht/TlyIs0!$ITǞ 4oP@S= 43&Nh'M\80hi,4N NNI^8Aa ~&A[4-:bIڤqA7$mQHڦqA8Ҁ6jZYىm8?Mڪq(A mrӃ6cѠm`jv},ham84MDl жv"AmTU%W 5R :@['4 z\+hӝmQ@km܃@;6|m"%h ( G`h ( K`hs˹G6~&A{%01hA}: O# mf ɏ7h(A;uD1]ʜA[%s`󗯇@>7h{x5G ;8hW>wN{hfB 5Q4&ǿK#[̄n]4?dI}.̻BLH' .OkCJcuCJBoE##^` ?S'v&WDHwPD=w>GǛL~2N''47V?J9^V聍ԸK=6?y96OS';OmϹOM ΑsOj-0ha$PƓ}YpnkYc|Fzu`v~F[.?&}(m@QI20UǦ]Z6V(L>jUJ?hҢ fGaTR:wd 41W֢t:#]b?D+]B_s`j;\*[U\U'֢{C ⧋'Ԣ*jхhE;T*Ԣhzra-z7ԯs@-c#Vs@1d~X*uB?4!9VV趂BJEB*O%dH.RVVi*ur2?4r CZrTr a ВK<.k*] rҵZ'C@+sP>װ^nH ejբeZYlM +էEf(*oeHmO|["S# ,C4;H8.-Z4P>-Z>3jhR'CQE]bH +թ%$THzQ;(]E =όZ:?1E$Z|ft +ibP^NOv,+u14&;xÖdϒRa~Ġhrǐx aJ E$5 :˂tݥݯb89Ir=uН%{#54D3RGR,? IAW[wp @g3E3GlhFjIVbS49PR^-'V[}~KANbГQ'ŠzP\S4:Lb^=Ql!~qyDbkhIvqyD!Q\^=Vb$Ҹzti(kHp$5|Ġ]忋>Jp$vufI@^gf#yy QjokN$qy]Ŧ8a==.(;<.&-߃j5i >."95i9!Q\N=vq9D~W"˩'Zxߒ\ q4|=.& j򸜚trjӤM)t?.R]\NԘ٧l'ϥϥ6i:Q.!Q\> Z|J*qŀ7R˥TOWZ\JϕzWwGK6CqP@\.g3KB_0GBSPr)%\Jf5BjfJO. q}ţT{P@ QP.;(U؇X sG`" K 铯8~1rr;Dj$0K5_q&AkJJ dj#+)HB<7:)I{dВGpg;1[JȆ'uJȆ'yJ+M:|'uaGC4DNi|>Hi)@T'G= dԫ Y>4K@V]QJ?ɨ8'UW\I!.dM(9!^nI !-h/w'A\ #"M(3qߧ[%%ݘ@'>]4ӯ1wDCZB?dstGvQ\GM6Oⶏ|8 qq'P>G1Bľq4Ԍz71}Y8)u>Ycia9:]wxG>5|Lּ~B!|*F̰r[S?3w>_4Kޞ;#nJ==\A?4x|?? rO$üMR #o^*TdޠmO hr>)+}RWJ]RSJ]RSJ#=R:OJ#w?@;}hv8=m!=Rm~1z*A;x(hy~̣>}Jà*Alah1a Ц#qP6qmЖg ڴy@ D6m:Ul:лm<͖XІC A5-h'hfC  ڬyA<ㅃjz6;^72]O?12ն̠6j#ꖖ>@k[ZrJZҲ>UYVyZ9MAp.@Nm <=>wjV;sSO kt@POźPwGqHd8i/՝ۋYjfj!̠qV=J2svu8^@DEױ>R!~:Cz i}YRv=+A?ɮ|q}:|F8B_n XIENDB`DdJ  C &Acsa_cabYf>Q%:wD~nYf>Q%:wDPNG  IHDRAA|vPLTE///䍍]]]ή&ubKGDH cmPPJCmp0712Om%IDATHՕW@ Gc\` 궠u]2({.7dwoV}|LԯוˏdhN@Vt ?LHBFH rG9Uym]9>) BbO t$,i$IBHRV]j&m"KW#5Ӟ1쮒-P:}z: ?E b$|Wc 7@AGL`^a]Й:YHp:ĊmVM*AEG_2IbKxT\zH`7zOx8( "@ա}\vJש'tYƩ$`p}TAe7P$9{[סfDRb CM{"Ҕb '࣓hzc}X94cشDͥ@9 gDx^ͺ!2sFKD6=a ~GA rAk]ٸO?y{`'Dz&.Tl0bRE7vU?XÿVN*xr'-IENDB`bDdg g 1H  S $GAulb_kD*(O~n_kD*(PNG  IHDRΏ sRGBgAMA a cHRMz&u0`:pQ<PLTEٟ pHYs\F\FCAIDATx͑8`V&h=+ g"8r `_#)S#A3(b"T>tPͮoSjߨw~CsWM|TeMw^{Wu%eQ^'3_/^<|)xRtBtB~"yٙOoޘxJO|"x& ?2y'W.Kdos/}>/{yΞ}6/{yܳg͏2esϞ}.? y'!<2y<:x*3cQǻ:|}7SXw92sxe9gsuUg𳚧}?yzgz^i^zFi^zFi ti~,])_t)w:$xwb 2Zx(dj}_ydQ/Ϗ+Ku"4#oKx_SgyWG^/]Z}c ީz6|^y h?(t|_:M?W[+Vy8OT[ O *|: ?K&4md> M3*s ?R>7M8fIH>JWo23|+DFN Ay'lÎ4U{$⻡3QuNcà^j4<|Hc<6 JǒöE 06@‡xޞD=+lDasbށŏ& kdAQL,_Wa3gi @4:{- c7mYSsh`i̬r1JGeӁ$24L{$ciX%1O)40|0$N Pǹ&SǫNi⧩;_v¡{XK. g8+9>N['7dL\9$9zݥlq>ΓK+|\%uG㉲8|&US!P2>_Cvс֨4SQj]ZNO,"m\>>N'c8GiG }̨sW^<5N_mfJZfTROSɛJ ~s T6s>) Q* GR?tUQai=Ql5>CR݈aǣ=gzz<0NQU'*g:IIszNXSGy+Wr'P,>r|DQq5ytB\<]xxrppV\ <(܄*ᗋ.gS~?G=WF)᧫S5Ïǧ)|~Sy`ø S_ÚQ=Q~P;_P~oQ?_Q>HJsV]y{t=?`|cE~zap?a|giߏ>V~o;_~#|"Cxsݓ*žƧ-xǣsO~8`~?<>aż55`qwW>7'ȯ{'^ݎ'?· rߐOWop[U~9 oޞx):rѪ&f|zρ|;~ߦ|rU_nMʧ˯#d>8d~OSV7mgS}~ɼBö|{:?1f|:ތ?Ʒ7v3obޞ#~:;? ~8"~| 탼]/~ ߇|>çB~ =mx{ߊ?ȷ]o W?~?~$߇%wO???_?????wOo#/g׼~~ou|{?}? SE6|{%?j=ۧxw.?﵌ދFg~)ț$w.dJ>^~:ZKR~&`hB𭘋?Mt8͉?⼫ʷ𳔟p~(橻 gOy{ϸۺB/܋1G~0KZIx}z|nF*9?qIĤ凄7}ħ52neG+>\7w;痔?ķ[_>w䓸'aᣳ;Mxs*Ajϯ MO!?Z)3c)ݪXrg>?]/U䳗;[_g.?~_Ƿb5sB| |~/'8t|.3uﲘ%h ;o;F SS @~OQx Hw?Ly t5xY~)'/ \ ]S;y{`>Dؼo(}KAcXſ^ y d!~ ٿw[dc??僂:z>N6dZ!ݛ7`14vά!y>lFyw+¯~|`׵W7כ*3n{g?#Qx[[o=@}5?a#oyW?bt=?`o|#;4VN}|Y9gW5痾 ߡ<|y󳚟Q~B_((Ā{MVSzr|3VɿVx!FoxyŲレ}b޼׮zVw9^/ޓ W} S9Cr\jx(/^{;K Vsx͟M|xP.NM _\2lm֖w$uCWbgyOӁW ?@ڎ|+^Bx ߨ,뭤o-[W]'~pY?^#cphG΂7$?ǓD~~c%y N7$?;z4n Gu?vW$?d+` oT$|tVቡM籡h|WwII#ͯ k{1C|TLf*9GVlbq^uY}P݇i3Su#bmщa GCVexSMXr(#- _oYX<†'Ց X*"|TC->ZuwBm# EA=jG12 eQ*JZfT9V{&iGuLSᣲ7gzF`mc4)8GIR :SyN r6x\ >J !/{IB>NRSA.(<_V>iSn`FC>Sf(Kk~\wN;QLJjҢå,}KnyyR^yq݅qW^G/O}/R>N0$+39>)[;1_3/$Q.|\'Gъ11ʖqwQ.|"=I$Be'O,T&3F)ķ?VM8sHOZC &2zK=$KI''2͗>Y§U' *I$H&|-V'}w7z()?R4'ҧ~I'ad$FcY@KLdʧ3J=ͼ$R>-|kso*4 t|y x1OU{L{iAj7N t>͡@̬OIs7~tFa8 '/o]G,|1~T><Ț^2Ƽ wB>/Aa[Ïc_.%gIZG*}l֌RZ'd7'~~!9jXGY^XG6c;aW(J{32R?{ɇ+30h,QΣ#/$F>`xgT;󋴷vrO}( >3:e6 ~Nf3}ϢmWݶKv~޶1';3U#mٜYmW2[rz +=NsJ~Jw%M,_'{-O.fXwjw5?W;=_#z=_#l?^z[—^_—-R񾔧?_zܳT/މ rz0|@'?lC% +͗,<_|*^|sV ^|v_xL ^*mg]86tY6 >gF|ʆ}[4P:냵<^|'Ky&"<_fuB&/_wMM^^zCU~ϳsyi1?g=W2+sCs?Le ΋f)wK쳿%ϝ{ /}AM<~f/IxYלsϺIO>Q#Engineering Spec FHH e Balloon TextCJOJQJ^JaJB'B eComment ReferenceCJaJ8"8 e Comment TextCJ@j!"@ eComment Subject5\4@B4 eHeader  !4 @R4 eFooter  !:@b: C Footnote TextCJ@&@q@ CFootnote ReferenceH*FV@F <FollowedHyperlink >*B* ph33KLTU`LKLMVWXYbcqr\]lm%&AB.;GYy $%Q p 7 8   y z   , < L \ r  : F d x 1F`u #0=JR]mnv!_);Ri{2BQRlmt/z{.u@pb>y-yt()}~rsTU9FXjw"#z{ U 3 0 00 0@0 0L 0 0 0 0 0 0@0@0 0L@0 0M@0 0@0 0Y@0 @0@0r 0Yr 0r@0r 0r@0r 0r@0r 0r@0r 0r@0r 0Yr@0r 0r@0r 0&r 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0 Br 0 Br 0 Br 0 Br@0r 0r@0r 0r@0r 0r 0r 0r 0r 0r@0r 0r@0r 0r@0r 0r@0r 0r@0r 0r@0r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0L r 0L r 0L r 0L r 0L r 0L r 0L r 0L r 0L r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r@0r 0 r 0dr 0dr 0dr 0dr 0dr 0dr 0dr 0dr 0dr 0 dr 0 dr 0 dr 0 dr 0 dr 0dr 0dr 0dr 0dr 0r 0r 0r 0r 0dr 0[r 0[r 0[r 0[r 0[r 0[r 0[r 0[r@0r 0r@0r 02r 0Mr 0Mr 0Mr 0Mr0r 02r 09r0r 02r 0r 0r 0r 0r 0r 0r 0r 0r 0r 0r 0 r 0 r 0 r 0 r 0 r 0r 0r 0r0r 0r0r 0r0r 0r0r 0r0r 0r0r 0r 0r 0r 0r 0r 0r 0r0r 0r0r 0 r0r 0 r0rD 0 r 0X r 0X r 0X r 0X rKLTU`LKLMVWXYbcqr\]lm%&AB.;GYy $%Q p 7 8   y z   , < L \ r  : F d x 1F`u #0=JR]mnv!_);Ri{2BQRlmt/z{.u@pb>y-yt()}~rsTU9FXjw"#z{ U !!?"@"""""######4$5$N$O$$$$$$%%'%?%O%g%%%%%&&E&W&X&&&&&''!'1'G'H''''(-(P(|(}((())))K*L***F+G+++++e,f,,,U.V.....//+/,///00000000:1;1t1u1112228393;3<3>3?3A3B3D3E3F3G3R3S3T3x3|3}33330000 00 0L 0 0 0 0 0 000 0L0 0M0 00 0Y000r 0Yr 0r0r 0r0r 0r0r 0r0r 0r0r 0Yr0r 0r0r 0&r 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0 Br 0 Br 0 Br 0 Br0r 0r0r 0 r0r 0 r 0r 0r 0r 0r0r 0 r0r 0 r0r 0 r0r 0 r0r 0r0r 0z r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0F r 0F r 0F r 0F r 0F r 0F r 0F r 0F r 0F r 0 r 0r 0r 0r 0r 0r 0r 0r 0r 0r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r0r 0z r 0nr 0nr 0nr 0nr 0nr 0nr 0nr 0nr 0nr 0 nr 0 nr 0 nr 0 nr 0 nr 0nr 0nr 0nr 0nr 0r 0r 0r 0r 0nr 0{r 0{r 0{r 0{r 0{r 0{r 0{r 0{r0r 0r0r 0Rr 0mr 0mr 0mr 0mr0r 0Rr 0{r0r 0Rr 0r 0.r 0.r 0.r 0.r 0.r 0.r 0.r 0.r 0.r 0 .r 0 .r 0 .r 0 .r 0 .r 0.r 0.r 0.r0r 0r0r 0r0r 0r0r 0r0r 0r0r 0r 0r 0r 0r 0r 0r 0r0r 0r0r 0 r0r 0 r0r 0 r 0{r 0{r 0{r 0{r0r 0r0r 0 r0r 0 r0r 0 r0r 0r0r 0"r0r 0"r0r 0"r0r 0"r0r 0r0r 05$r 0O$r 0O$r 0O$r 0O$r 0O$r 0O$r 0O$r 0O$r 0O$r 0 O$r 0 O$r 0 O$r 0 O$r 0 O$r 0O$r 0O$r 0O$r0r 05$r 0X&r 0X&r 0X&r 0X&r 0X&r 0X&r 0X&r 0X&r0r 05$r0r 05$r 0'r 0'r 0'r 0'r0r 0r0r 0}(r0r 0}(r0r 0}(r0r 0}(r0r 0}(r0r 0}(r0r 0r0r 0+r0r 0+r0r 0 r0r 0 r0r 0 r0r 0.r0r 0 r0r 0/r0r 0/r0r 0/r0r 0 r0r 0r0r 00r0r 00r0r 0r0r 0u1r00@000@0X00@0X00@0X00@0X00@0@0@0@0@0@0@0@0@0@0X00(KLTU`LKLMVWXYbcqr\]lm%&AB.;GYy $%Q p 7 8   y z   , < L \ r  : F d x 1F`u #0=JR]mnv!_);Ri{2BQRlmt/z{.u@pb>y-yt()}~rsTU9FXjw"#z{ U !!?"@"""""######4$5$N$O$$$$$$%%'%?%O%g%%%%%&&E&W&X&&&&&''!'1'G'H''''(-(P(|(}((())))K*L***F+G++2833 0 00 0@0 0L 0 0 0 0 0 0@0@0 0L@0 0M@0 0@0 0Y@0 @0@0r 0Yr 0r@0r 0r@0r 0r@0r 0r@0r 0r@0r 0Yr@0r 0r@0r 0&r 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0Br 0 Br 0 Br 0 Br 0 Br@0r 0r@0r 0r@0r 0r 0r 0r 0r 0r@0r 0r@0r 0r@0r 0r@0r 0r@0r 0r@0r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0L r 0L r 0L r 0L r 0L r 0L r 0L r 0L r 0L r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r 0 r@0r 0 r 0dr 0dr 0dr 0dr 0dr 0dr 0dr 0dr 0dr 0 dr 0 dr 0 dr 0 dr 0 dr 0dr 0dr 0dr 0dr 0r 0r 0r 0r 0dr 0[r 0[r 0[r 0[r 0[r 0[r 0[r 0[r@0r 0r@0r 02r 0Mr 0Mr 0Mr 0Mr0r 02r 09r0r 02r 0r 0r 0r 0r 0r 0r 0r 0r 0r 0r 0 r 0 r 0 r 0 r 0 r 0r 0r 0r0r 0r0r 0r0r 0r0r 0r0r 0r0r 0r 0r 0r 0r 0r 0r 0r0r 0r0r 0 r0r 0 r0r 0 r 0g r 0g r 0g r 0g r0r 0r0r 0!r0r 0!r0r 0!r0r 0r0r 0#r0r 0#r0r 0#r0r 0#r0r 0r0r 0#%r 0=%r 0=%r 0=%r 0=%r 0=%r 0=%r 0=%r 0=%r 0=%r 0 =%r 0 =%r 0 =%r 0 =%r 0 =%r 0=%r 0=%r 0=%r0r 0#%r 0F'r 0F'r 0F'r 0F'r 0F'r 0F'r 0F'r 0F'r0r 0#%r0r 0#%r 0(r 0(r 0(r 0(r0r 0r0r 0k)r0r 0k)r0r 0k)r0r 0k)r0r 0k)r0r 0k)r Z00 00 DZZZ]M %#,7:?;;#*.5<@ITY[TK V Y q \ & 7zdmlz)#9&&((*+5,,W.!//|0033467788u9:F;x;;!"$%&'()+,-/012346789:;=>?ABCDEFGHJKLMNOPQRSUVWXZ\]; 223 @  @H 0(  0(  B S  ? OLE_LINK1,3T.3_ _\ $$3$$39*urn:schemas-microsoft-com:office:smarttagsplace8*urn:schemas-microsoft-com:office:smarttagsCity +o222229393;3;3<3<3>3?3A3B3D3E33329393;3;3<3<3>3?3A3B3D3E333'01;LLQ R V Y Vuoo{{ ((o)p)))++F+F+G+G+++222222839393;3;3<3<3>3?3A3B3D3E3G3H3O3P3}33333 uuoo{ ((o)p)))++F+F+G+G+++22273839393;3;3<3<3>3?3A3B3D3E3333 x2E0xR8U0xR`uv ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH()^`;o(hHPART hh^h`;o(hH.^`56o(hH.^`56o(hH.^`56o(hH.00^0`56o(hH) PP^P`o(hH) ^`o(hH() ^`o(hH()^`;o(hHPART hh^h`;o(hH.^`56o(hH.^`56o(hH.^`56o(hH.00^0`56o(hH) PP^P`o(hH) ^`o(hH() ^`o(hH() ^`o(hHPART  hh^h`o(hH.`P`^``P56o(hH. P^`Po(hH. P^`Po(hH. pPp^p`Po(hH)  P ^ `Po(hH) ^`o(hH() ^`o(hH()2E 8U`uvw15Bc6Lzv ,a3D6V}9HQ#C%~U%o% &Z&@()b>+}X+X4,eb,x/1 14&5682/8t;@<J<=cC>$@Cu D BFCF-I2BIdLxNfOPMlRSbU Y.Yj\#[__dUegi?@ABCDEFGHIJKLMNOPQRSTUVWXYZ[\]^`abcdefghijklmnopqrstuvwxy{|}~Root Entry F,\!Data _m41TablezxWordDocument4SummaryInformation(DocumentSummaryInformation8CompObjq  FMicrosoft Office Word Document MSWordDocWord.Document.89q ii-112-232ins-b - Littelfuse - 8.1U3